STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ETH1 doesn't work on stm32mp135

Hi, I designed a board with stm32mp135 and YT8531 phy chip. The ETH1 is not working and ETH2 is work good. They all output 125Mhz from phy to mac. But the ETH1 has reset dma failed. I had measure the 125Mhz is correct on phy side.Below is my dts code...

SChen.19 by Associate II
  • 3140 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP157FAD schematic design

hiI am working on a project using stm32mp157fad.For the project created using stm32cubemx and stm32cubeide, I created a custom image by referring to the site below and uploaded it to the sd card using the dd command.But openstlinux is not booting up ...

_legacyfs_online_stmicro_images_0693W00000bkVSlQAM.png _legacyfs_online_stmicro_images_0693W00000bkVTsQAM.png
KNam.2 by Associate II
  • 3709 Views
  • 4 replies
  • 0 kudos

Resolved! eMMC HS200 clarification

Hi there,we are in the process of developing a product based on the STM32MP151F which will be USB powered (USB 2.0 device).We are aiming to have it connected to an eMMC for mass storage and we would like to achive the highest R/W speed which should b...

Resolved! Can't flash SD card on STM32MP157-EVAL

I have a STM32MP15X-EVAL board MB1262C-01 with a MB1263B-04 CPU-board on it (MP157AAA3). I'm following the instructions from 'STM32MP15_Evaluation_boards_-_Starter_Package'Boot 0,1,2 jumpers are OFF, JP1 is removed. USB connected to CN4 (ST-Link) an...

NKall.1 by Associate II
  • 4237 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.