2023-05-15 10:29 AM
STM32MP157C-dk2
I am trying to update the Board using SUART3 (Pins PB10, PB12) over STM32CubeProgrammer. The connection to STM32CubeProgrammer is established successfully. Unfortently after downloading the fdbl-boot (tf-a-stm32mp157c-dk2-uart.stm32)
the failure appears while system tries to start from downloaded part.
See console:
-------------
19:25:00 : File : tf-a-stm32mp157c-dk2-uart.stm32
19:25:00 : Size : 216.38 KB
19:25:00 : Partition ID : 0x01
19:25:00 : Download in Progress:
19:26:23 : File download complete
19:26:23 : Time elapsed during download operation: 00:01:23.074
19:26:23 : RUNNING Program ...
19:26:23 : PartID: :0x01
19:26:23 : Start operation done successfully at partition 0x01
19:26:54 : Timeout error occured while waiting for acknowledgement.
------------------
Are there any limitation to the UART used by given bootloader? Or what are other reasons which might be related to the issue?
2023-05-16 12:27 AM
Hi @WSief.1 ,
Could you please share the log from serial console and details of ecosystem used ( CubeProgrammer and OpenSTLinux version )
Thanks,
Olivier
2023-05-16 1:29 AM
2023-05-16 11:16 PM
Hi @WSief.1 ,
The log file you sent is still the one from CubeProgrammer on host side.
The one I have asked for is the serial log from target, usually on UART4.
Anyway, in the one you sent I can read :
"10:26:06:639 : Error: File does not exist: H:\W.Siefried\von JSLT\Piedrafita\Starter-Package\WMS\STM32MP157C-DK2/arm-trusted-firmware/tf-a-stm32mp157c-dk2-usb.stm32
10:26:06:713 : Error: TSV flashing service failed"
That's look to point to an obvious issue in your tsv file or binary file organization.
Typically path of such firmware in Starter Package is this:
\images\stm32mp1\arm-trusted-firmware
Why -usb flavor while I understand you want to program with UART3 ?
And, for my curiosity, why you program a DK2 with UART3 ?
On this board preferable path is USB, then UART4.
Olivier
2023-05-17 2:01 AM
The described error is not related for issue (startup of programmer)
The configuration is loaded at 10:26:17:482 : Read TSV File....
I will check UART 4 and provide information.
In general: I am using UART3 as alternative to USB to check a developer board where USB currently not working. This eval board is used for verification purpose.
2023-05-17 3:49 AM
Log of UART4:
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
NOTICE: Board: MB1272 Var2.0 Rev.C-01
INFO: PMIC version = 0x10
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using UART
INFO: Instance 3
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
ASSERT: plat/st/common/bl2_io_storage.c:329
Exception mode=0x00000016 at: 0x00000001
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.