STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 I2S_CKIN as source for PLL4

Hi there,in order to have an externally generated clock for our LTDC peripheral we decided to use the I2S_CKIN as the reference clock for PLL4 on our customized STM32MP157CAC board. Reference manual and STM32CubeMX are showing that this opportunity e...

HAL9000 by Associate
  • 1587 Views
  • 0 replies
  • 1 kudos

Resolved! stm32mp135 PA10 as tim1 ch3 pwm

Hi,I have a problem with the configuration of PA10 of stm32mp135 to work as pwm of TIM1_CH3. I also make an experiment to disable completely timer and PWM and I also can't control this pin using gpioset. In the documentation I saw that this pin is de...

MWoło.2 by Senior III
  • 4861 Views
  • 7 replies
  • 0 kudos

Resolved! libqmi build for STM32MP157

I'm building libqmi for the STM32MP157 and getting an error  at this point in the build GISCAN Qmi-1.0.girTraceback (most recent call last):File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-v...

edwardmcl by Associate II
  • 2889 Views
  • 2 replies
  • 0 kudos

STM32MP1 boot fail in TF-A

Hi all,We design the custom board use ST32MP157 base on the design of STM32MP157-DK2 kit. We use the SD card for booting. The image and device tree is custom base on example of STM32MP157-DK2 kit. The board has a issue when booting via SD card. This ...

Resolved! stm32mp135f trusted vs optee efficiency

Hello, For some time I testing STM32MP135f with 1GHz CPU clocking. I was able to generate optee OpenStLinux but I see a lack of CPU efficiency. I'm curious what is the difference in efficiency between trust and optee. If I use the trusted option the ...

MWoło.2 by Senior III
  • 2281 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.