2023-06-28 3:06 PM
Hi,
I have a slight problem with st-image-weston.bbappend.
In my meta-layer in folder /recipes-st/images/ I add an st-image-weston.bbappend to install a few packages I intend to have.
And now something is strange, after adding a new package to install into rootfs the packages start to compile but not install on rootfs.
Content of my st-image-weston.bbappend
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
inherit populate_sdk_qt5
IMAGE_INSTALL += " \
qtbase-dev \
qtbase-mkspecs \
qtbase-tools \
qtdeclarative-qmlplugins \
qtquickcontrols2-qmlplugins \
qtwayland \
gstreamer1.0 \
gstreamer1.0-plugins-good \
"
CORE_IMAGE_EXTRA_INSTALL += " \
net-tools \
openvpn \
systemd-networkd-configuration \
netplan \
networkmanager \
iproute2 \
ppp \
usb-modeswitch \
usbip \
ppp-dialin \
libiio \
packagegroup-st-demo \
sox \
libnfc \
sdcard-raw-tools \
"
IMAGE_ROOTFS_MAXSIZE = "950000"
Finally, many packages are not installed for instance USB gadget DHCP server, ppp etc.
For stm32mp15x such update mentioned file works. Why not work for 13x?
Thanks for any hints
BR Michal
Solved! Go to Solution.
2023-06-29 2:30 PM
Small update,
on the sd-card packages are installed, so the problem I have is related to EMMC. I think We can close this topic.
2023-06-29 2:30 PM
Small update,
on the sd-card packages are installed, so the problem I have is related to EMMC. I think We can close this topic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.