STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP133 OTP Alternate QSPI Boot

Hello, In order to use the non-default QSPI boot locations, my understanding is port0-port3, 4 signals need to be defined in OTP words 3, 5, and 6 based on a similar question about SDMMC1 discussed here:https://community.st.com/t5/stm32-mpu-products/...

Jasper by Associate II
  • 4900 Views
  • 4 replies
  • 0 kudos

stm32mp135 - pcm5102a - sai1a

Hello,I try to connect a popular Arduino board PCM5102a with my board which is base on STM32MP135.I read some documentation from the linkhttps://wiki.st.com/stm32mpu/wiki/ALSA_overviewhttps://wiki.st.com/stm32mpu/wiki/Soundcard_configurationhttps://w...

MWoo2_0-1688975337399.jpeg
MWoło.2 by Senior III
  • 8970 Views
  • 11 replies
  • 1 kudos

Resolved! S24_LE support on I2S of STM32MP1 line

Hi,what's the state of the S24_LE format support on the STM32MP1 line of boards? It seems that S16_LE and S32_LE formats are supported on the I2S dai, however S24_LE is rather unavailable. Is there a way to somehow enable it (maybe through Cube MX) o...

AJank.2 by Associate III
  • 3152 Views
  • 2 replies
  • 1 kudos

STUSB1600 (USB-C) Alternatives

Hey,I am designing a board based on the STM32MP157F using the OSD32MP157F SOM as a base. I want to have a usb-c connector acting as a host and/or as hs_otg. Reviewing the DK boards schematics I see that the STUSB1600 is being used. I also see on the ...

Sindel by Associate
  • 1597 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP15x ADC Oversample

Could someone point me to some documentation about how to control the oversampling for ADC1 and ADC2 for the STM32MP157C?    Using OpenSTLinux 4.1.0, buildroot.   I looked around but couldn't find anything. Thanks!

Macdog by Associate III
  • 2407 Views
  • 1 replies
  • 0 kudos

Switch uboot logs to usart6

Hello, I have a board based on the stm32mp153a and I'm trying to get it to boot, unfortunately I can only access USART 6 while it seems that uboot only tries to interact using uart4.In my dbs file I have overridden usart6/status to be "okay" instead ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.