STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OpenAmp_TTY_echo not creating rpmsg0|1

Hello,Searched around but couldn't find a similar issue.Please point me to one if one exist. I have a custom board with the stm32mp157c mounted. Board works fine, trying to communication between the m4 and a7 processor using the rpmsg devices. I have...

mantwih by Associate III
  • 2017 Views
  • 1 replies
  • 0 kudos

Resolved! Troubleshooting WLAN brcmfmac43430 firmware load failure on STM32MP1:Hardware vs Config

Hi there, I am working on a custom board based on OSD32MP157F. The pinout is very similar to the stm32mp157f-dk2 with the main difference that the Murata LBEE5kL1BX-883 is connected to sdmmc3 instead of sdmmc2 and that there is no ethernet peripheral...

KChar.1 by Senior
  • 8910 Views
  • 6 replies
  • 0 kudos

Resolved! stm32mp135 pwm dts

Hi,can some share dts configuration which allows you to bring up the PWM, timer etc?I do something like  pwm_regulator { compatible = "pwm-regulator"; pwms = <&{/soc/timer@40002000/pwm} 3 500000 0>; regulator-min-microvolt = <1016000>; regula...

MWoło.2 by Senior III
  • 2202 Views
  • 1 replies
  • 0 kudos

Issues in OPTEE (bootloader)

I am trying to boot my STM32MP153C over cubeProgrammer to load data in EMMC0.Unfortantly the programm is failing in OPTEE Part (Second file to download). Here is the UART log:NOTICE: CPU: STM32MP153CAA Rev.ZNOTICE: Model: STMicroelectronics STM32MP15...

WSief.1 by Associate II
  • 4265 Views
  • 3 replies
  • 1 kudos

STM32MP1 (Kirkstone version) openocd-stm32mp-native execution error in YOCTO project

Hello, I am new to yocto project, I am trying to build a yocto project based on the stm32mp1(a development board from a vendor based in Germany). I am building core-image-full-cmdline. My Ubunutu version is Ubuntu 22.04.2 LTS.My build configurations ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.