2023-06-22 8:41 AM - last edited on 2023-06-29 12:26 AM by Olivier GALLIEN
I'm building libqmi for the STM32MP157 and getting an error at this point in the build
GISCAN Qmi-1.0.gir
Traceback (most recent call last):
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/bin/g-ir-scanner", line 98, in <module>
from giscanner.scannermain import scanner_main
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/scannermain.py", line 35, in <module>
from giscanner.ast import Include, Namespace
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/ast.py", line 29, in <module>
from .sourcescanner import CTYPE_TYPEDEF, CSYMBOL_TYPE_TYPEDEF
File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/sourcescanner.py", line 34, in <module>
from giscanner._giscanner import SourceScanner as CSourceScanner
ImportError: /home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/gobject-introspection/giscanner/_giscanner.cpython-310-x86_64-linux-gnu.so: wrong ELF class: ELFCLASS32
make[4]: *** [/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/share/gobject-introspection-1.0/Makefile.introspection:156: Qmi-1.0.gir] Error 1
So it has a problem with _giscanner.cpython-310-x86_64-linux-gnu.so: wrong ELF class: ELFCLASS32
Any idea why?
Solved! Go to Solution.
2023-06-30 6:43 AM
Hi @edwardmcl ,
I see that you are trying to compile with developper package ?
Can you please clarify what you want to achieve and how ?
libqmi seems to be already part of Yocto Distribution as part of meta-oe layers.
If not integrated by default I guess it might be straighforward to add it.
Did you look in that direction?
Olivier
2023-06-30 6:43 AM
Hi @edwardmcl ,
I see that you are trying to compile with developper package ?
Can you please clarify what you want to achieve and how ?
libqmi seems to be already part of Yocto Distribution as part of meta-oe layers.
If not integrated by default I guess it might be straighforward to add it.
Did you look in that direction?
Olivier
2023-06-30 6:47 AM
I'm building because I want to use libqmi for the STM32MP157. I wanted to do this within the Developer package but if it's already there in Yocto I'll explore that option. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.