STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA Buffer Index with Multi-Channel ADC

Hello!I am using the CortexM4 coprocesor on the STM32MP157F-DK2 to measure multiple ADC channels and update a control loop based on the values. I have set up ADC1 using the DMA2 in circular mode to read channels IN1, IN2, and IN4. I have a buffer set...

jutoroa by Associate III
  • 2946 Views
  • 2 replies
  • 0 kudos

STM32MP1 - MAC address

Greetings,  I have a few STM32MP1 boards. One of which I have configures the OS on, and custom applications.I copied the SD card and put it in another one.  The MAC address is the same. I read an STM article about the MAC address and "fuse sense 0 57...

Resolved! Inquiry about Obtaining a Custom Name for Virtual Serial COM Port on STM32MP13X Device

Hi,We are currently working on a project that involves utilizing the STM32MP13X MPU. Our device operates in both ACM and Mass Storage Mode, and we would like to inquire about the process of obtaining a custom name for the virtual serial COM port gene...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.