STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spidev_test

Hi,I like to use spidev_test tool:https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev#Installation_on_your_targetI am following this guide for compiling the tool by developer package:https://wiki.st.com/stm32mpu/wiki/How_...

pjanco by Associate
  • 2456 Views
  • 0 replies
  • 0 kudos

Occasional missing TxRxCpltCallback callback on SPI DMA transfer on the ARM-M4 of an STM32MP1

We are experiencing an issue where, in approximately 1 in 1000 cases, we don't get a TxRxCpltCallback callback after starting a SPI DMA transfer from an ISR on the ARM-M4 (coprocessor). The transfer appears to have taken place as all the bytes are re...

jamescc by Associate II
  • 1993 Views
  • 0 replies
  • 0 kudos

Resolved! stm32mp15x emmc reboot stuck-up

Hi,I have a problem with hanging up my board occasionally when an issue from the console reboot.I read about and the internet says this is a problem with the EMMC memory's power cycle.So I followed by a linkhttps://github.com/orangepi-xunlong/openwrt...

MWoło.2 by Senior III
  • 2220 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP151 emmc OTP configure

Hello. We already have a custom board based on STM32MP151CAD3 with an eMMC. The following pins are different with default eMMC pins.SDMMC2_CMD: PA0SDMMC2_D1: PB7 As not default pins are used, we need to update OTP value. Here are my result. OTP3 = 0x...

Kernel panic after flashing

Hello, I built an image with the following configuration by using the ST wiki pages:STM32MP157D-DK1 Evaluation BoardYocto KirkstoneSTM32MP1-Ecosystem-v4.1.0meta-java layer (branch kirkstone)I have used the following command to create an image:./creat...

enienws by Associate
  • 1658 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.