2023-07-18 11:34 AM
Greetings,
I have a few STM32MP1 boards. One of which I have configures the OS on, and custom applications.
I copied the SD card and put it in another one. The MAC address is the same. I read an STM article about the MAC address and "fuse sense 0 57 2" shows me the correct MAC address. So it must be in software somewhere. Where?
2023-08-01 2:26 AM
Hello @jgauthier ,
Yes this is a typical issue when we copy a SD card into another, it results in this MAC address error.
To tackle it, you will need to stop in U-Boot shell, and process an "erase env" to delete the config with the MAC address, and get a new one.
Hope it will help you,
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.