STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Yocto mickledore SIGN_TOOL

HelloIn the new version of Yocto release mickedore, SIGN_TOOL variable needs to be specified to sign TF-A binary which should corresponds to STM32CubeProgrammer signing tool https://wiki.st.com/stm32mpu/wiki/Signing_toolPractically, how can we set th...

syedelec by Associate III
  • 5363 Views
  • 6 replies
  • 1 kudos

What if M4 RAM is too small?

When porting applications from single core M4's equipped with FLASH, the RAM associated with M4 in MP1 is supposed to cater for both RAM and former FLASH needs. It won't fit. How to overcome this if M4 code/data size cannot be reduced?

PeterL by Associate III
  • 3054 Views
  • 5 replies
  • 0 kudos

Resolved! STLINK-V3MODS for STM32MP1 Compatibility

Hello,I am in process of designing my own STM32MP1 powered device. I was wondering if I can use STLINK-V3MODS as a drop in replacement for ST-LINK/V2-1 in STM32MP157-EVAL reference design. I need the Virtual COM interface embedded in device.-Mark

mhd0425 by Associate II
  • 2567 Views
  • 2 replies
  • 1 kudos

QEMU on stm32mp157

I want to emulate the stm32mp157 on qemu. I have been taking the kernel image and initrd from yocto build, but it is not loading the kernel. using the following commandqemu-system-arm \-M virt -smp 8,sockets=1,cores=4,threads=2 -m 4G \-cpu cortex-a7 ...

Resolved! STM32MP157FAD1

Hello,I would like to ask you few questions since I have some unclearances about STM32MP157F MPU:1. If 933MHz DDR3L RAM was connected to the MPU according to the schematic, will the MPU automatically underclock it to max 533MHz?2. Is it possible to c...

filip1785 by Associate II
  • 2641 Views
  • 1 replies
  • 1 kudos

RPMSG SDB driver failure on M4 restart

Recently I got a problem with RPMSG driver when M5 coprocessor restarts. Thanks to https://community.st.com/s/question/0D53W00000936uRSAQ/kernel-panic-with-pollselect-syscalls-on-virtual-uart-devices-to-m4-core-when-m4-watchdog-restarts?t=16321442601...

mishuk by Associate III
  • 4095 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.