2026-01-21 3:05 AM
I have a custom board with stm32wba65 processor. I also have an RFM95 LoRa module. I need to add LoRaWAN capability. I tried adding I-CUBE-LRWAN into my CubeMX but was not able to load it (not a recognised package).
How can I get an ST or Semtech approved LoRaWAN stack into my project?
Please do not suggest I use stm32WL processor.
Solved! Go to Solution.
2026-01-21 12:39 PM
Hi @Andrew Neil
I escalated the request to the responsible team for review and to push that the I-CUBE-LRWAN package will be available (Internal ticket number: 225628).
I will post updates here as soon as I have more details.
2026-01-27 1:36 AM
I very much look forwards to a full and comprehensible manual.
2026-01-27 1:44 AM
I can now see the 'Documentation' tab again on the Product Page.
The User Manual is:
UM2073 STM32 LoRaWAN® Expansion Package for STM32Cube
2026-01-27 1:51 AM - edited 2026-01-27 1:52 AM
Also noted in the thread I linked earlier is that the LoRa(WAN) code all comes from Semtech.
So you could try going direct:
"LoRa Basics Modem/Modem-E is an easy-to-use software library that simplifies the development of LoRaWAN® end-nodes in the ISM Sub-GHz and 2.4GHz bands for worldwide interoperability. It provides developers with an event-driven interface at a high level of abstraction. The Software stack is compatible with TS001-LoRaWAN L2 1.0.4 and Regional Parameters RP2-1.0.3 specifications."
https://www.semtech.com/products/wireless-rf/lora-basics-modem
via: https://www.semtech.com/products/wireless-rf/software-library-protocol-solution
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.