STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Enrolling P-NUCLEO-LRWAN3 on Loriot Server

I have enrolled the gateway and the end node of my PNUCLEO lrwan 3 on Loriot server, but when I view the boot log on my Terra Term terminal, I observe that the end node does not join the server, returning JOINED FAILED.I made sure the end node and th...

Screenshot (64).png

Resolved! Fraudulent Power Claims in STM32WB55 Wireless SoC

Dear STMicroelectronics Team,I am writing to strongly condemn the way power consumption values are presented in the STM32WB55 datasheet.When I choose a wireless SoC, I do so because of its wireless capabilities. If I only needed a microcontroller, I ...

Resolved! I2C1 has decided to stop working?

NUCLEO WB55For an unknown reason I2C1 has just stopped working. The BLE & UART are working but the boards (I've tested on 2 identical boards) are no longer talking to the sensors via I2C.When I scope them up the traces for SCL & SDA are both flat lin...

Using Nucleo-f411re with LoRa ra2 sx1278

Hello,I’m new to embedded systems and currently learning STM32 + LoRa.I’m using two NUCLEO-F411RE boards and two RA-02 (SX1278) LoRa modules. My goal is to establish basic point-to-point communication.I initially tried using a LoRa.h library, but I c...

osPriorityNone used in STM32WB example projects

Hello,Looking at the HRS FreeRTOS example applications code for STM32WB55, I see several task configured with osPriorityNone as priority.This priority level is defined as meaning 'no priority, not initialized' in cmsis header.Why is it used here ? Ho...

NOLFF.1 by Associate II
  • 183 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WBA55 VBAT PROBLEM

I have a project for a battery-powered clock using the STM32WBA55 chip. The battery is replaceable; the device can sit unused on a shelf for up to 4 months without the battery. Since the STM32WBA55 doesn't have VBAT or VRTC pins, how can I keep the b...

YBAYR.1 by Associate III
  • 293 Views
  • 1 replies
  • 1 kudos

Resolved! stm32wba65 and I-CUBE-LRWAN

I have a custom board with stm32wba65 processor. I also have an RFM95 LoRa module. I need to add LoRaWAN capability. I tried adding I-CUBE-LRWAN into my CubeMX but was not able to load it (not a recognised package).How can I get an ST or Semtech appr...

SLevi1_0-1768993411104.png
SLevi.1 by Senior
  • 1096 Views
  • 13 replies
  • 1 kudos

STM32WL blocked in RTC initialization

Hi, I'm working with a STM32WL5MOC with the STM32Cube FW_WL V1.4.0. In my main.c I have this initialization: MX_GPIO_Init(); MX_DMA_Init(); MX_RTC_Init(); MX_LPUART1_UART_Init(); MX_USART1_UART_Init(); MX_ADC_Init(); MX_CRC_Init(); MX_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.