2026-04-28 8:37 AM
The product page and datasheet only mention BLE Core 6.0 but don't call out channel sounding support explicitly like other BLE features. Is it actually supported?
Solved! Go to Solution.
2026-04-28 9:13 AM
Yes, the STM32WBA6 is Bluetooth LE 6.0 certified. However, it does not support Channel Sounding.
Please note that Channel Sounding is not only a software feature; it also requires specific hardware/IP support in the device architecture, which is not available on STM32WBA6.
Kind regards,
Petr
2026-04-28 9:13 AM
Yes, the STM32WBA6 is Bluetooth LE 6.0 certified. However, it does not support Channel Sounding.
Please note that Channel Sounding is not only a software feature; it also requires specific hardware/IP support in the device architecture, which is not available on STM32WBA6.
Kind regards,
Petr
2026-04-28 1:26 PM
Thank you for the fast reply Petr!
Is channel sounding something that you expect ST to support with a different device in the future?
2026-04-28 4:04 PM
Yes, there will be a device with channel sounding in the future - stay tuned!
Regards
/Peter
2026-04-29 1:17 AM - edited 2026-04-29 9:28 AM
Hi @TechUmNu and welcome to the Community,
For projects requiring channel sounding feature, you can also consider alternative or future platforms such as the STM32WBA2 lines, which are planned to address this use case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.