2022-04-22 2:24 AM
Hello, I am testing two STM32WL55. I have two NUCLEO-WL55JC2 demoboards.
I'm using the example code provided in the LocalNetwork_Concentrator and LocalNetwork_Sensor demos.
In the basic configuration, I cannot manage to have a communication distance range of more than 1m...
Do you know what the maximum ranges of these Nucleo boards?
Is there a setting to configure or is it a problem with the hardware design?
Thank you
2022-05-02 7:10 AM
Hello @joe_lambord ,
Which region have you configure via the AT command on the concentrator side ?
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.