cancel
Showing results for 
Search instead for 
Did you mean: 

Why now ERR_UNKNOWN_HCI_COMMAND return value to aci_hal_get_anchor_period()?

Scott Löhr
Senior II

Hello - I was using the results of aci_hal_get_anchor_period() just a few months ago, but now in v1.13.3 BLE_full_stack, it is returning ERR_UNKNOWN_HCI_COMMAND. Is there some command that needs to be sent to enable getting the anchor period? If there is no way to successfully invoke this in v1.13.3, please - what is the last version in which it was enabled?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Remy ISSALYS
ST Employee

Hello,

Indeed, other modifications need to be done inside the application to be compatible with BLE full extended, the better solution is to wait release v1.14.0. The aci_hal_get_anchor_period() command will be reintegrated in the BLE full stack for release v1.14.0.

Best Regards

View solution in original post

3 REPLIES 3
Remy ISSALYS
ST Employee

Hello,

Indeed this command isn't supported in BLE Full stack v1.13.3. To use this command, you shall used the BLE Full Extended stack.

In order to use BLE Full Extended stack, it is necessary to adapt the scatter file in the BLE applications as:

  • The RAM_A shared range shall be reduced to memory range [0x20030000:0x200307FF]
  • The Mail-box buffers(MB_MEM1, MB_MEM2) shall be located in RAM_B shared defined in memory range [0x20038000:0x2003A7FF]
  • The RAM_B shared shall be added to Total_RAM_region
define symbol __ICFEDIT_region_RAM_SHARED_start__ = 0x20030000;
define symbol __ICFEDIT_region_RAM_SHARED_end__   = 0x200307FF;
 
define symbol __ICFEDIT_region_RAM_B_SHARED_start__ = 0x20038000;
define symbol __ICFEDIT_region_RAM_B_SHARED_end__   = 0x2003A7FF;
define region RAM_B_SHARED_region = mem:[from __ICFEDIT_region_RAM_B_SHARED_start__   to __ICFEDIT_region_RAM_B_SHARED_end__];
 
define region Total_RAM_region  = RAM_region | RAM_SHARED_region | RAM_B_SHARED_region;

Best Regards

@Remy ISSALYS​ thanks for this insight. I made simple linker file change and programmed the v1.13.3 BLE full-Extended stack. Startup procedure as expected until this step where it hangs here:

static void APP_BLE_Init(void)
{
    HCI_TL_HciInitConf_t Hci_Tl_Init_Conf = {
        .p_cmdbuffer = (void *)&BleCmdBuffer,
        .StatusNotCallBack = BLE_StatusNot
    };
 
    hci_init(BLE_UserEvtRx, &Hci_Tl_Init_Conf);
 
    SHCI_C2_Ble_Init_Cmd_Packet_t ble_init_cmd_packet =
    {
        .Header = { .MetaData = {0} },  // Does not need to be initialized by the user.
 
        .Param = {
            .pBleBufferAddress = NULL,  // NOT USED - shall be set to 0.
            .BleBufferSize = 0,  // NOT USED - shall be set to 0.
            .NumAttrRecord = CFG_BLE_NUM_GATT_ATTRIBUTES,
            .NumAttrServ = CFG_BLE_NUM_GATT_SERVICES,
            .AttrValueArrSize = CFG_BLE_ATT_VALUE_ARRAY_SIZE,
            .NumOfLinks = CFG_BLE_NUM_LINK,
            .ExtendedPacketLengthEnable = CFG_BLE_DATA_LENGTH_EXTENSION,
            .PrWriteListSize = CFG_BLE_PREPARE_WRITE_LIST_SIZE,
            .MblockCount = CFG_BLE_MBLOCK_COUNT,
            .AttMtu = CFG_BLE_MAX_ATT_MTU,
            .SlaveSca = CFG_BLE_SLAVE_SCA,
            .MasterSca = CFG_BLE_MASTER_SCA,
            .LsSource = CFG_BLE_LSE_SOURCE,
            .MaxConnEventLength = CFG_BLE_MAX_CONN_EVENT_LENGTH,
            .HsStartupTime = CFG_BLE_HSE_STARTUP_TIME,
            .ViterbiEnable = CFG_BLE_VITERBI_MODE,
            .Options = CFG_BLE_OPTIONS,
            .HwVersion = 0,  // Reserved for future use - shall be set to 0.
            .max_coc_initiator_nbr = CFG_BLE_MAX_COC_INITIATOR_NBR,
            .min_tx_power = CFG_BLE_MIN_TX_POWER,  // Range: -127 .. 20
            .max_tx_power = CFG_BLE_MAX_TX_POWER,
            .rx_model_config = CFG_BLE_RX_MODEL_CONFIG
        }
    };
 
    ASSERT_RETURN(SHCI_Success == SHCI_C2_BLE_Init((void *)&ble_init_cmd_packet));  // Starts the BLE Stack on CPU2.
}

So it would seem that some parameter in the SHCI_C2_Ble_Init_Cmd_Packet_t is not good for the Extended stack, even as it is working fine with the Full stack. Can you give any more hints on how to make the Full stack run, or do we have to wait for v1.14. in June?

Remy ISSALYS
ST Employee

Hello,

Indeed, other modifications need to be done inside the application to be compatible with BLE full extended, the better solution is to wait release v1.14.0. The aci_hal_get_anchor_period() command will be reintegrated in the BLE full stack for release v1.14.0.

Best Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.