2024-04-09 9:27 AM
At this link, using "Windows PowerShell" on Windows 11, https://github.com/STMicroelectronics/STM32CubeWL
using method 4, failed.
git clone --recursive --depth 1 --branch v1.3.0 https://github.com/STMicroelectronics/STM32CubeWL.git
Cloning into 'STM32CubeWL'...
remote: Enumerating objects: 13497, done.
remote: Counting objects: 100% (13497/13497), done.
remote: Compressing objects: 100% (6783/6783), done.
error: RPC failed; curl 92 HTTP/2 stream 5 was not closed cleanly: CANCEL (err 8)
error: 6756 bytes of body are still expected
fetch-pack: unexpected disconnect while reading sideband packet
fatal: early EOF
fatal: fetch-pack: invalid index-pack output
==============================
re-try using method 1, also failed
git clone --recursive https://github.com/STMicroelectronics/STM32CubeWL.git
Cloning into 'STM32CubeWL'...
remote: Enumerating objects: 22375, done.
remote: Counting objects: 100% (7677/7677), done.
remote: Compressing objects: 100% (4026/4026), done.
error: RPC failed; curl 92 HTTP/2 stream 5 was not closed cleanly: CANCEL (err 8)
error: 6465 bytes of body are still expected
fatal: early EOF
fetch-pack: unexpected disconnect while reading sideband packet
fatal: fetch-pack: invalid index-pack output
git clone --recursive https://github.com/STMicroelectronics/STM32CubeWL.git
Solved! Go to Solution.
2024-04-24 12:41 AM
Hello @David_
I'm not able to reproduce this. Can you check your Proxy configurations.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-09 9:59 AM
Can you clone anything else from GitHub?
ie, is this a general GitHub problem, or something specific to this ST repo?
2024-04-09 10:10 AM
I guess this is the traditional issue of software. Instruction was correct at time when they are written. Then, break when time go by with updates.... Apprenetly, STM32Cube has been doing a good job to auto update as it flashes at right-bottom. The green "code" button worked as designed, downloaded most modules and some need manual download, as stated on instruction.
2024-04-24 12:41 AM
Hello @David_
I'm not able to reproduce this. Can you check your Proxy configurations.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-24 2:03 AM
Many thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.