STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 issue with BLE Connection

Hi,Everything was working fine with my stm32wb55 until it suddenly decided to stop working. Now when I tried to upload the example firmware for ble p2pserver and connect to the web application provided by stm, i am able to connect, but the web applic...

Resolved! learning lrwan1

hello im doing a school project using a Nucleo-F411RE with a I-NUCLEO-LRWAN1 expansion, anyone got a good text or video tutorial how i connect the two boards?im using the stm32cubeide

Resolved! Zigbee enabling and disabling question with STM32WB5MM-DK

Hi All,I am new in Zigbee programming and I like to get some starting point to make server-client model. Up to now, I am using STM32CubeIDE tool to program with .ioc file to setting up the HW. Eventually I would like to use STM32WB5MMG processor and ...

YJ99 by Associate II
  • 1560 Views
  • 1 replies
  • 0 kudos

Resolved! Custom STM32 BLE Application with ThreadX - Azure RTOS

Hi everyone, I am trying to build my custom BLE application with CubeMX (v6.11.0) and STM32CubeIDE: v1.15.0 using a STM32WB55 with FW package: v.1.19.0.Due to its other functions I would like to use ThreadX for that. However, when generating code wit...

Lo by Associate II
  • 2785 Views
  • 3 replies
  • 1 kudos

Resolved! STM32WB BLE and EEPROM casuing HardFault

Hi CommunityHope you guys are well. I am trying to implement Bluetooth and emulated eeprom working. i have followed the ble_heartrate_eeprom_emul example and i got blue tooth and eeprom emulation working, the problem i am having is when the EEPROM em...

Resolved! Can someone explain the function of SX_FREQ_TO_CHANNEL?

Hello,I'm working on an application that uses the NUCLEO-WL55JC development board. I was looking in the SubGHz_Phy_PingPong example code, and I noticed a macro called SX_FREQ_TO_CHANNEL. To use this macro, it seems you input the carrier wave frequenc...

AJ_1 by Associate III
  • 3442 Views
  • 7 replies
  • 3 kudos

Resolved! STM32WLE5JC Receiver Chain

Hi !   I read the datasheet, and it says: "The receive chain comprises a differential low-noise amplifier (LNA), a down-converter tolow-IF by mixer operation in quadrature configuration". 1. What is the GAIN and the NF of the diff. LNA ?       1.a Is...

KTrot.1 by Associate II
  • 1463 Views
  • 1 replies
  • 0 kudos

Resolved! Creating a LoraWAN server on an stm32 chip

I am making a device that is to take pulse outputs which have been converted to wireless LoRaWAN signals, and convert it back again into a hardwire pulse output. For the receiving device, I intend to use a modem board PN 109990166 connected to an STM...

How to calculate impedance matching for STM32WLE5 RF network?

I am attempting to compute an impedance matching network by following the guidelines outlined in the ST Application Note - AN5457.However, on page 24, the formula and calculations appear unclear to me due to the presence of a negative value under the...

Levan_2-1707896427471.png Levan_3-1707896650413.png
Levan by Associate III
  • 2142 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.