2017-05-03 2:42 AM
Does anyone have any experience with the current consumption when using B-L072Z-LRWAN1 (STM32L072 and LoRa board) with i-cube-lrwan 110?
I can't get the current consumption below below 1.1mA no matter what i try. In lowpower (stop) mode all pins are set as analog, clocks are disabled, debug is off.
- I checked the device going into STOP mode
- Configured all non-connected pins to GPIO_MODE_ANALOG, GPIO_NOPULL
- Configured connected pins (UART, etc.) to GPIO_MODE_OUTPUT_PP, GPIO_NOPULL, and set to zero
I also stopped the debug clock in the ARM:
__HAL_RCC_DBGMCU_CLK_ENABLE( );
HAL_DBGMCU_DisableDBGSleepMode( );
HAL_DBGMCU_DisableDBGStopMode( );
HAL_DBGMCU_DisableDBGStandbyMode( );
Also TCXO is Off.
Still the current consumption is above 1 mA.
Anyone out there that managed to get the current down?
Thanks!
#lora #b-l072z-lrwan1Solved! Go to Solution.
2017-12-12 4:05 AM
Hello,
I have a technical question about the sleep current consumption. The results you get here is around 4 uA. Thats ok, but less consumption should be possible.
I configured my B-L072Z-LRWAN:
-
TCXO connect to PA12
- Compile the code with no DEBUG, no TRACE, no SENSOR_ENABLED,
- LED7 disconnected by opening SB18
- SB37 removed to release the RESET
Then I get 1.6 uA with some repetitive current peaks in sleep mode. This leads also to around 4 -5 uA (Measured with the Power Analyzer)
Now the when I look at the datasheet The MCU(
STM32L072CZ)
should consume 0.855 uA with RTC on and the SX1276 consumes 0.2 uA in sleep mode.So when looking at the datasheets I should get a sleep mode of around 1.055 uA.
How can I reach this value? Is it possible with the development kit (B-L072Z-LRWAN)?
Are there some official sleep current values of the
B-L072Z-LRWAN
? I cant find them..Kind Regards,
Lukas
2017-12-13 12:52 AM
Hi.
Comment out the HW_AdcInit () function.
// HW_AdcInit();
2017-12-13 4:32 AM - edited 2024-01-24 1:53 AM
Posted on December 13, 2017 at 12:32
There is another (potential) leakage path which is not documented - and doesn't even have a solder bridge or jumper to disconnect it!
>:(
See:
https://community.st.com/0D70X000006SsOaSAK
EDIT (Jan 2024): That link seems to be broken (by a forum update?) - try this:
2017-12-13 4:35 AM
With SB19 intact, or JP2 fitted, there seems to be some significant current draw on VDD_USB_LRA ...
2017-12-14 1:18 AM
That was it! Thanks. I am down at 1.2 uA in sleep mode.
Is there any possibility to go lower? Use another sleep mode or something?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.