2017-12-15 8:53 PM
Hello everyone, this is a problem regarding my DISCO-L072CZ-LRWAN kit which I am using for a project of mine.
I am using the LRWAN expansion kit for LoRa functionality while I am also trying to add up a UART as UART1 on Pin 9/10. While using this UART, I am trying to use the HAL drivers especially HAL_UART_Receive function which receives N number of character and has a timeout given by the user which I am giving as 0x00FF. Internally this function takes sysTick using Get_HAL_Tick() but as the LoRa function has initialized all LL drivers, the getting systick function from HAL does not work. Which means that there will be no timeout and I have to specify the number of characters to be received, which is bizarre.
I hope you understood my problem. Please try and help with solution or any other alternative.
If you have any solution for UART which solves this problem please reply.
#b-l072z-lrwan1 #b-l072z-lrwan1Solved! Go to Solution.
2017-12-16 8:39 AM
The LRWAN implementation uses the RTC over SysTick, but it is possible to implement/enable SysTick if you need/want to.
Unless you've got a bunch of experience I wouldn't try to mix HAL and LL stuff up to much. I would strongly recommend reading the Reference Manuals so you know how the underlying hardware works as this will provide a lot of clarity about what the software needs to do.
The LRWAN/VCOM implementation is a bit of a mess, there is a lot of blocking code compounded by the way the CM0+ NVIC works. I ended up reworking most of that code to use the status and data registers more directly, and providing some more effective FIFO buffering via the IRQ Handlers.
2017-12-15 10:18 PM
Either go to debug mode to figure out how to cascade the Systick interrupt to all functions needing them, or use a simple unused STM32 Timer to build a programmable timeout event that you use in your main loop to abort UART (ie: Make your own timeout).
2017-12-16 4:35 AM
SARTHAK KELAPURE wrote:
I am trying to use the HAL drivers especially HAL_UART_Receive function
But your thread title says LL Drivers - so which is it?
Do you actually need the timeout?
2017-12-16 8:39 AM
The LRWAN implementation uses the RTC over SysTick, but it is possible to implement/enable SysTick if you need/want to.
Unless you've got a bunch of experience I wouldn't try to mix HAL and LL stuff up to much. I would strongly recommend reading the Reference Manuals so you know how the underlying hardware works as this will provide a lot of clarity about what the software needs to do.
The LRWAN/VCOM implementation is a bit of a mess, there is a lot of blocking code compounded by the way the CM0+ NVIC works. I ended up reworking most of that code to use the status and data registers more directly, and providing some more effective FIFO buffering via the IRQ Handlers.
2017-12-18 10:45 PM
Well thank you. I ended up mixing the HAL and LL drivers and it works as of now. Even I am going to remake vcom.c again. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.