NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on December 16, 2017 at 05:53Hello everyone, this is a problem regarding my DISCO-L072CZ-LRWAN kit which I am using for a project of mine.I am using the LRWAN expansion kit for LoRa functionality while I am also trying to add up a UART as UAR...
Posted on May 03, 2017 at 11:42Does anyone have any experience with the current consumption when using B-L072Z-LRWAN1 (STM32L072 and LoRa board) with i-cube-lrwan 110?I can't get the current consumption below below 1.1mA no matter what i try. In low...
Posted on October 30, 2017 at 17:25 Is it possible to 'manually' configure the Tx Power level using theI-CUBE-LRWAN v1.1.2 software? I can see that the End_Node demo enables Adaptive Data Rate: /* ! *Initialises the Lora Parameters */ sta...
Posted on September 15, 2017 at 16:29Hi All,I am using STM32l073 nucleo board with module. I am unable to get power more than 14.6 dBm while transmitting data packet. On my other device i am able to get 19 dbm of power using same sx1272 module.I tri...
Posted on December 01, 2017 at 05:42Hi All, I have a custom designed PCB with STM32L073RZ + SX1276 LoRa transceiver + LIS2DH12 MEMS accelerometer. LoRa chip uses SPI2 and sensor uses SPI1 interfaces. Interrupts for the sensor are not being used. The...
Posted on November 16, 2017 at 23:52I purchased three B-L072Z-LRWAN1 nodes yesterday and started my long awaited experimenting. The distance while maintaining stable communication between two B-L072Z-LRWAN1 nodes is a bit of a dissapointment. After ...
Posted on November 03, 2017 at 15:02Hello,Using 2 WM-SG-SM-42 modules which are parts of I-NUCLEO-LRWAN1 I am trying to establish point to point communication without LoRaWAN. I have updated the AT commands firmware to 3.0 and I am following the exa...
Posted on October 27, 2017 at 22:01Is the I-NUCLEO-LRWAN1 extension board plug-in compatible with the STM32F429 Nucleo-144?#lorawan #nucleo-144
Posted on October 25, 2017 at 15:37I'm developing application with P-NUCLEO-LRWAN1 modifying I-CUBE-LRWAN software.But i could not trigger CAD (Channel Activity Detection) function. And i'm not sure that interrupt for CAD_DONE (DIO3) is enabled or n...
Posted on October 20, 2017 at 19:16I have: B-L072Z-LRWAN1 Discovery board (based on muRata module)P-NUCLEO-LRWAN1 Pack (Nucleo-64 board with Semtech SX1272 bare chip add-on).I-CUBE-LRWAN firmware pack, v1.1.2Keil MDK for STM32L0/F0, v5.24aMultiTech...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.