2019-10-28 12:40 PM
Are there any application notes or references about a border router used with a Thread network because I hadn't found any.
Solved! Go to Solution.
2019-10-30 9:50 AM
I assume that as long as the new board is supporting the Thread protocol on one side and an internet connection on the other side using either a wired connection or a separate Wi-Fi module, it should be OK.
2019-10-29 10:13 AM
The border router use case is not supported by the Thread stack provided for the STM32WB.
The Thread + Ethernet or wifi connectivity is missing to fulfill this feature.
2019-10-30 2:07 AM
Is there any way to connect a raspberry pi to the network and use that as the border router?
2019-10-30 9:50 AM
I assume that as long as the new board is supporting the Thread protocol on one side and an internet connection on the other side using either a wired connection or a separate Wi-Fi module, it should be OK.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.