NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I feel uncomfortable with this: on page 26 AN5165 there are shown layers purposes. In particular, written, that INNER1 used as "grounding under the RF zones", but on images below (Figure 33) under RF this layer is deleted and as reference used anothe...
In Application note AN5165 exist example of 2-layer PCB (MB1427). What the project it is? I can't find it on STMicroelectronics website.
Hi,I am using STM32WB55 to develop a 802.15.4 application. I browse the two 802.15.4 examples, but there is no documentations like 802.14.5 Application Programming Interface. Can you provide those 802.14.5 documentations?Thanks,
Here is the log of the error:13:22:22 : Memory Programming ...13:22:22 : Opening and parsing file: P-NUCLEO-WB55.Nucleo_Thread_Coap_DataTransfer.elf13:22:22 : File : P-NUCLEO-WB55.Nucleo_Thread_Coap_DataTransfer.elf13:22:22 : Size : 114550 Bytes13:22...
My graduation project is about design a lora node and communicate with user using with lora gateway. I will take antenna sx1276 gps and stm32l0 or stm32wb.
Hello,I have STM32WB set from workshops that I borrowed from my work.The problem is both pcbs are not recognised in DFU mode. I connected stm32f4-discovery and it's recognised correctly.I'm Linux Mint 19 user and I have followed CubeProgrammer's inst...
HiI tried using the P2P_SERVER profile of the STM32WB55XX example (with atollic).When pushing on CONNECT on my mobile, I expect seeing the LED and BUTTON services as written in the example documents, but I see the 2 PRIMARY SERVICES (Generic Attribut...
Error 14:24:08 : Time elapsed during download operation: 00:00:00.82614:24:08 : Verifying ...14:24:08 : Read progress:14:24:08 : Error: Data mismatch found at address 0x08000000 (byte = 0xE0 instead of 0x00)14:24:08 : Error: Download verification fai...
Hi, I am having issues reinitialising the BLE stack after waking up from sleep. I am initialising it the exact same was as normal power on. Upon waking up and calling the TL_Enable() function, a shci_notify_asynch_evt it not being received. Is there...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.