STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Adjust ZbZclClusterCommandReq callback timeout

Hello,I am looking how to shorten the timeout and/or failure entering of the callback.I am using ZbZclClusterCommandReq(cluster, &req, callback, arg). I currently have my own ACK timeout implementation, however, the callback still is entered with eit...

ISLTG by Associate III
  • 572 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with Extended Erase Command on STM32WB55RG via USART1

Hi support, I’m currently working with a Nucleo-WB55RG board, and my goal is to perform a firmware update using an ESP32 as the host. The ESP32 is connected to the STM32 via USART1 (PA9 and PA10).The sequence followed is : 1. Connect to the bootloade...

Xem by Associate II
  • 996 Views
  • 4 replies
  • 1 kudos

I-CUBE-LRWAN Abandoned?

In another thread:@vicrr wrote:The Cube LRWAN package you mentioned it not the latest one and has not been updated for years.We recommend you to use the STM32CubeWLSo what about platforms other than WL? Are they abandoned?@vicrr 

Resolved! I-NUCLEO-LRWAN1 Still Supported?

Hi all,As part of a uni project we are developing a LoRaWAN Weather station project.We have free access (the team is operated on a limited budget) to a I-NUCLEO-LRWAN1 board. This appears to be a very good option as the board has all the integrated s...

sr71brd by Associate
  • 637 Views
  • 2 replies
  • 0 kudos

Resolved! Issue Building CM0Plus project

Hello,Context: New to stm and HAL. Creating a new dual-core STM32 project on a NUCLEO-WL55JC1 board. Starting from cubeMX generated code with basically only RTC initialized on Core M4. Using STM32CubeWL Firmware package v1.3.1 . M4 builds and loads g...

lame_stmr by Associate III
  • 2227 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.