2025-07-15 1:40 AM
Hello,
I’m working with the X-NUCLEO-WB05KN1 shield and a STM32 Nucleo board.
My goal is to make a simple demo: Toggle an LED on the board by sending a command from my smartphone. Display something on the smartphone when pressing the User button on the Nucleo.
I understand that I need to update the shield with the BLE_Transparent_Mode_STM32WB05_location_essential firmware from X-CUBE-WB05N_V2.0.0.
However: Which exact firmware binary should I flash for this purpose?
Which smartphone application should I use to communicate with the board?
Is nRF Connect sufficient or is there a recommended alternative?
Thanks in advance for your help!
2025-07-15 1:49 AM - edited 2025-07-15 2:08 AM
@sheulisback wrote:Is nRF Connect sufficient
It could certainly do it, but it's a competitor's app - so this is not the place for support with that!
2025-07-15 1:54 AM
Hello,
Thank you for your reply.
The smartphone application is not mandatory for me, I’ll just use my phone as a tool.
I mainly need to know which application or tool you recommend to interact with the WB05KN1.
Could you please advise?
Thanks again!
2025-07-15 2:06 AM
Yes, the nRF one is perfectly fine.
The beauty of standards like BLE is that they are totally agnostic to the hardware: so all the app sees is BLE Characteristics, Services, Advertising, etc - it neither knows nor cares anything about what chips your device uses.
The point is just that it's a competitor's tool - so you won't find any support for it here.
2025-07-15 2:12 AM
In that case, could you suggest a non-competitor application that I can use, so I can also get support here if needed?
I’d rather use a tool aligned with your recommendations, if that’s not an issue.
Thanks again!
2025-08-08 12:08 AM
Hello @sheulisback
To select the mobile application, you are going to use for your app. I suggest you have a look at the Connectivity:BLE smartphone applications - stm32mcu.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.