2025-08-01 2:13 AM
I am using the BLE_p2p_Server_ext example on a stm32wba55cg and i want to use ADC_Channel_2 as a way of voltage measurements.
My current setup:
I use a new adc handle:
ADCCTRL_Handle_t adc_channel2_handle =
{
.Uid = 2,
.State = ADCCTRL_HANDLE_NOT_REG,
.InitConf =
{
.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1,
.Resolution = ADC_RESOLUTION_12B,
.DataAlign = ADC_DATAALIGN_RIGHT,
.ScanConvMode = ADC_SCAN_DISABLE,
.EOCSelection = ADC_EOC_SINGLE_CONV,
.LowPowerAutoPowerOff = DISABLE,
.LowPowerAutonomousDPD = ADC_LP_AUTONOMOUS_DPD_DISABLE,
.LowPowerAutoWait = DISABLE,
.ContinuousConvMode = DISABLE,
.NbrOfConversion = 1,
.ExternalTrigConv = ADC_SOFTWARE_START,
.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE,
.DMAContinuousRequests = DISABLE,
.TriggerFrequencyMode = ADC_TRIGGER_FREQ_LOW,
.Overrun = ADC_OVR_DATA_OVERWRITTEN,
.SamplingTimeCommon1 = ADC_SAMPLETIME_814CYCLES_5,
.SamplingTimeCommon2 = ADC_SAMPLETIME_1CYCLE_5,
.OversamplingMode = DISABLE,
},
.ChannelConf =
{
.Channel = ADC_CHANNEL_2,
.Rank = ADC_REGULAR_RANK_1,
.SamplingTime = ADC_SAMPLINGTIME_COMMON_1
}
};and add a new task id to my task_id_list:
CFG_TASK_VOLT_MEASI register the new task to my sequencer:
UTIL_SEQ_RegTask(1U << CFG_TASK_VOLT_MEAS, UTIL_SEQ_RFU, MyVoltageReadTask);and I have a timer that wakes my device every ~30 seconds. I then set the task as active:
UTIL_SEQ_SetTask(1U << CFG_TASK_VOLT_MEAS, CFG_SEQ_PRIO_0);this is my MyVoltageReadTask:
void MyVoltageReadTask(void)
{
uint16_t adc_value_raw = 0;
ADCCTRL_Cmd_Status_t Cmd_Status = ADCCTRL_UNKNOWN;
// Pause BLE temp task to avoid conflict
UTIL_SEQ_PauseTask(1U << CFG_TASK_TEMP_MEAS);
/* Enter limited critical section : disable all the interrupts with priority higher than RCC one
* Concerns link layer interrupts (high and SW low) or any other high priority user system interrupt
*/
UTILS_ENTER_LIMITED_CRITICAL_SECTION(RCC_INTR_PRIO<<4);
/* Request ADC IP activation */
Cmd_Status = ADCCTRL_RequestIpState(&adc_channel2_handle, ADC_ON);
/* Get temperature from ADC dedicated channel */
Cmd_Status = ADCCTRL_RequestRawValue(&adc_channel2_handle, &adc_value_raw);
/* Request ADC IP deactivation */
Cmd_Status = ADCCTRL_RequestIpState(&adc_channel2_handle, ADC_OFF);
/* Exit limited critical section */
UTILS_EXIT_LIMITED_CRITICAL_SECTION();
// Resume BLE temp task
UTIL_SEQ_ResumeTask(1U << CFG_TASK_TEMP_MEAS);
// Do some calculation with the adc value...
}that process works and I can receive the adc value via advertisement on a different device. At -20°C and +50°C I have no problem. However if I use my stm32wba55cg at a temperature around 0°C it gets stuck and it stops advertising. I have multiple boards with the stm32wba55cg and all behave the same around that 0°C.
The only way to get it out of that is by resetting it externally or with a watchdog. Then it works for a undefined period of time until it gets stuck again.
If I remove the task from the sequencer and do nothing else with ADC4 everything works fine, even at those temperatures.
Does anyone else have issues with using ADC4 if temperature calibration is enabled or am I missing something?
Any help appreciated.
Solved! Go to Solution.
2025-08-08 4:13 AM
I changed from STMCubeIDE 1.17.0 to 1.19.0 and changed the BLE_p2pServer_ext example to the state of the 1.17.0 version. That seemed to do the trick. Currently multiple devices are continously sending and the watchdog is not triggering. I can not say if something changed on the watchdog or with the adc handling in 1.19.0.
I will close this ticket for now.
2025-08-04 12:07 AM
I checked to see if it had anything to do with moisture and condensation so i added a bunch of silica gel in to a bag with my pcbs but it had no effect.
Does anyone know what triggers the internal temperature calibration?
2025-08-08 4:13 AM
I changed from STMCubeIDE 1.17.0 to 1.19.0 and changed the BLE_p2pServer_ext example to the state of the 1.17.0 version. That seemed to do the trick. Currently multiple devices are continously sending and the watchdog is not triggering. I can not say if something changed on the watchdog or with the adc handling in 1.19.0.
I will close this ticket for now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.