STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Nucleo-WB05KZ power consumption

Hello I have a nucleo wb05kz programmed with BLE_Power_Consumption example project (STM32Cube_FW_WB0_V1.1.0 package) and i want to measure the current consumption.Following the UM3343, I removed the JP1 and JP2 jumpers and connected my power supply (...

Resolved! STM32WL55 and STM32WLE5 HW compatibility

Hi,I would like to confirm that STM32WL55 and STM32WLE5 are mutually HW compatible from the point of external circuitry? I.e. can we use either one in a PCB originaly designed for one of them w/o any modifications? (Yes, I checked both datasheets but...

MMici.1 by Associate III
  • 859 Views
  • 1 replies
  • 0 kudos

Low-power mode STM32WLE5

We are developing with the STM32WLE5JC6, everything works, but now we are trying to reduce current consumption. When using the "End node skeleton", it seems to work, however, we are trying to define our own skeleton, because we neither want the ADC n...

STM32WL33CC enters DeepStop but does not wake up

Hello everyone,I'm working on a project using the STM32WL33CC1, based on the example provided in the official ST GitHub repository:https://github.com/STMicroelectronics/STM32CubeWL3https://github.com/STMicroelectronics/STM32CubeWL3/tree/main/Projects...

SergioSI by Associate II
  • 1230 Views
  • 2 replies
  • 0 kudos

lora tx problem using hal lib

I am working on stm32wl5moc controller and lora tx is not working every  time radio status i am getting back is 5 instead of 6, below is the code snipet, and also check the full code attached with this post if (HAL_SUBGHZ_ExecGetCmd(&hsubghz, RADIO_G...

Resolved! LoRaWAN cubemx generated code is showing error

../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'1650 | ( MacCtx.McpsIndication.ResponseTimeout > 0 ) )| ^ The above error is occuring every time ,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.