NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on January 26, 2018 at 12:47Hi, i want to know, in which party of the script of STM32 discovery LoRa can i generate a message that i want to transmit ! ? Thanks#lorawan
Posted on November 03, 2017 at 17:27Hello everybody,Is there a way to import the I-CUBE-LRWAN software in Eclipse ? I'm facing many problems and cannot find a proper solution. Thanks in advance !#p-nucleo-lrwan1 #eclipse #i-cube-lrwan
Posted on January 13, 2018 at 01:59I am trying to run this End Node example in Visual Studio.but; hw_gpoi.h has these errors:[Clang IntelliSense] Error: unknown type name 'IRQn_Type' Lora_1 c:\vs2018\lora_1\inc\hw_gpio.h 86 also fails wi...
Posted on January 11, 2018 at 07:54 I have a Murata LoRa SOC from which I have made up a custom board and I am flashing code using UART which wasn't successful until help from https://community.st.com/people/Turvey.Clive.002 Now I am using stm...
Posted on January 09, 2018 at 17:43Hello everyone,I have made a custom board using Murata LoRa SOC and I am trying to flash it using Flash Loader Demo by STM and I am able to flash the code only once out of 10 times. The application shows 'Stopped W...
Posted on December 25, 2017 at 06:38Hello everyone,I am using Murata LoRa discovery board DISCO-072CZ-LRWAN. A simple queryWhen I put the STM32L072CZ (present in the board) to sleep, does that mean the SX1276 LoRa trans receiver also goes to sleep? ...
Posted on December 23, 2017 at 14:51Hello everyone,I have a general query about any embedded system. Whenever we use any communication device(maybe Bluetooth or WiFi or GSM), is it advised to use AT commands to control the device?Thank you in advanc...
Posted on December 22, 2017 at 06:36if is it possible then which memory are use for store the hex file.external flash or system flash?please suggest other option also.
Posted on December 19, 2017 at 15:26I have two queries for anyone who can help me,1)What is the maximum payload for US915_HYBRID, SF7, 125kHz BW for LoRa?2)I need an extra UART on stm32l072cz LoRa discovery board. Can anyone help with this.Please he...
Posted on December 15, 2017 at 15:42I am a beginner on stm32 microcontroller I am currently using Nucleo-L073RZ I am wondering if there is any code examples may help me to understand how to recieve data via Uart (TX,RX) and send it via Lora Network...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.