STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

OTA Update

Posted on September 26, 2017 at 08:34Hi Dear, We want Low Power With OTA update based  Micro-Controller Please Suggest me Which are the Best Solution. Thanks!Nitin Kanani #ota #stm32f

Why I got verry low RSSI from P-NUCLEO-LRWAN1?

Posted on September 07, 2017 at 09:14I use a P-NUCLEO-LRWAN1 and I-cube-lrwan End_node firmware. It was connect with Semtech lora gateway but rssi is very low and it have some lose of message from P-NUCLEO-LRWAN1.  please see result a picture below....

0690X000006089PQAQ.png 0690X000006089UQAQ.png

STM32CubeExpansion_LRWAN_V1.1.1 uses stale L4 HAL

Posted on August 26, 2017 at 01:17The LRWAN tree contains a very old L4 HAL tree, doesn't support L496, also lacks support for NUCLEO 32 and 144 boards.Ported in the V1.8.0 L4 Cube supplied HAL libraries.Got about 90% through a port of the SX1272MB2...

0690X000006042FQAQ.jpg

Send LoRa packet with AT command - b-l072z-lrwan1

Posted on June 12, 2017 at 15:37Hello,I am trying to use LoRa connectivity with the brand new b-l072z-lrwan1 discovery board. The End Node project works perfectly but I have an issue with the AT Slave project. When I try to send LoRa packet to my Mu...

How can I process to Make a DFU OTA

Posted on August 02, 2017 at 09:02I'm currently working on a BLE device. This device has no screen nor keyboard. It is using a STM32L0 and is connected to an application on android.I want to make a DFU (device firmware update) via bluetooth (OTA) so...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.