NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,Totally newb. I have a custom board with a STM32WB55CEU6. Connected over ST-LINK.I'm trying to upgrade FUS. Using stm32wb5x_FUS_fw.bin at 0x0807A000Everything seems to work fine until the very last step, where I get an error: FUS_STATE_IMG_NOT_FOU...
Hi community,I'm very new to STM32 wireless. I need some support.I followed the MOOC "STM32WB Getting Started Series: Part 12b, Lab. Receiving data from the phone " using Nucleo WBA55CG board. When I build the code, there were 0 error and 0 warning. ...
Hello STM32 Community,I accidentally erased the full firmware on my STEVAL-PROTEUS1 board (STM32WB5MMG). After that, I followed this process to recover:FUS firmware: Updated using stm32wb5x_FUS_fw.bin from STSW-PROTEUS (since FUS was missing in the o...
Hi,I'm having strange situation with mine BLE application on STM32WB5M module, i.e. Peripheral mode, which has implemented configuration characteristic (write with confirm) according by BLUEST protocol 00000000-000F-11e1-9ab4-0002a5d5c51b. Client rep...
Hi everyone,I'm working on a LoRa project using the STM32WL55JC1 microcontroller, and I'm looking to implement a self-healing mesh network with multiple repeaters.Could anyone suggest existing libraries, detailed tutorials (step-by-step preferred), o...
Ever since being forced to update STM32CubeIde, every time a change is made to the .ioc file and the code is regenerated the following errors show up.app_ble.c /** * Write the BD Address */ p_bd_addr = BleGetBdAddress(); ret = aci_hal_write_confi...
I've added the X-CUBE_AZRTOS-WB software pack and checked all the boxes for ThreadX but the RTOS ThreadX checkbox in STM32CubeIDE is disabled. Is something else required to use ThreadX on an STM32WB? Kindes regards
Hello.I'm trying to launch a minimal LoRaWAN project. CubeMX version 6.15.0. When using MSI RC clocking, the module works without issues. When attempting to use the TCXO, the module starts, packets are successfully transmitted to the server, but are ...
I want to use a USB connection on a STM32WBA65 processor, purely for debug purposes to get some info back to a PC on a virtual com port. The device will not be powered by USB.I don't want the processor to act as a host.Questions:Can the STM32WBA65 pr...
I would like to use STM32WB (NUCLEO-WB55) with eddystone and sleep periodically.I find examples about beacon and about power low mode but it's not easy merge them.I'm looking for an example.Thank youPaolo Preioni
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.