2025-08-09 4:42 AM
I want to use a USB connection on a STM32WBA65 processor, purely for debug purposes to get some info back to a PC on a virtual com port. The device will not be powered by USB.
I don't want the processor to act as a host.
Questions:
Solved! Go to Solution.
2025-08-12 3:57 AM
Hi @SLevi.1
STM32WBA65 integrates a USB HS peripheral.
You can check this example. You can refer to CAD resources.
If you are using USB type C only ( without power delivery), you need to connect CC1 and CC2 pins each to ground via 5.1 kΩ pull-down resistors (required for USB-C device detection).
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-12 3:57 AM
Hi @SLevi.1
STM32WBA65 integrates a USB HS peripheral.
You can check this example. You can refer to CAD resources.
If you are using USB type C only ( without power delivery), you need to connect CC1 and CC2 pins each to ground via 5.1 kΩ pull-down resistors (required for USB-C device detection).
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.