NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I followed the tutorial from this video: https://www.youtube.com/watch?v=6JPys9B497c to practice setting up BLE.After flashing to the NUCLEO-WBA55CG, the ST BLE Toolbox app still cannot detect the device.I also noticed that after it executes: UTIL_LP...
Dear Sir,I am working on reading values from 10 ADC channels of the STM32WB55CGU6 (WeAct Studio board). However, I am not getting the correct voltage readings. Please note the following details about my setup:I am using USB (Virtual COM Port) to prin...
Hello folks, I've seen a similar topic(link) on this forum, but it had no solution, I'll take my chance and see if you could offer me some tips on how to debug this. I've designed a custom "break-out" board for STM32WB5MMG and I'm trying to communica...
Hi, I'm facing an issue with waking the STM32WL55JC1 from Standby mode using RTC Alarm A. Setup: Using LSE as RTC clock source RTC and Alarm A are initialized correctly Alarm A interrupt works when not entering standby Wake-up via RTC Wakeup Time...
I followed the tutorial from this video: https://www.youtube.com/watch?v=6JPys9B497c to practice setting up BLE.However, after building the project I encountered the following error: crtn.o: missing C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/co...
Dear ST Support Team and Community Experts,I'm developing a BLE application using the STM32WB55 Nucleo board (P-NUCLEO-WB55) and observed unexpectedly low data throughput, requesting guidance on optimization.1. Issue DescriptionCurrent Rate:Modified ...
I have recently taken delviery of a custom board carring the SMT32WB5MMG SiP. This is the first time I have used this specific part in a custom design, but previously have been working with a SMT32WB55 development kit without any issues.In my design ...
Hi everyone, I couldn't find the application note on STM32WB0 MCU hardware development. Can I refer to AN5290 which is for STM32WB instead of the STM32WB0. If so, is there anything I would need to pay attention to for the STM32WB0 series? Or should...
Given that STM32WL product line seems to support Wi-Fi 802.11ah (HaLow) bandwidth and modulations. Would one be able to configure the radio to connect to such network?
Hi all, I'm setting up a custom board using the STM32WL33 device. I'm using four single-ended ADC inputs: ADC_VINM0, ADC_VINP0, ADC_VINM3, ADC_VINP3.I would like to use DMA and sequencer, adding TEMP and VDD as 5th and 6th conversions. I managed to g...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.