NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am unable to successfully put the STM32WB55 into Shutdown mode and then wakeup via either one of the WKUP pins or the RTC. I can get the WKUP pins to work if I use HAL_PWRex_DisableInternalWakeupLine, but then it won't wakeup via the RTC. If I om...
Hello! PCB Antenna for STM32WB shown in AN5129 Application note where used pcb stack-up with core 711.2 μm. Exactly the same antenna used in P-NUCLEO-WB55 (MB1355) where pcb thickness is ~1500 μm. How is it possible? How changes antenna parameters wh...
Hello,I'm developing an application based on B-L072Z_LRWAN1 hardware.If i Program my code on the evaluation board everyting works good. I can send and receive packets with LoRa.If I program it on my custom hardware (based on the evaluation board) ev...
Hi,We designed a product using STM32WB series for BLE application. In our case we didn't follow any impedance for antenna due to size constraints. Now we are facing BLE advertising problem.Is the problem with impedance or any other. Kindly guide us ...
I'm using a WB55 Nucleo board and setting up a BLE connection with a 2nd WB55 Nucleo board using aci_gap_create_connection(). The connection succeeds and I am able to transfer data between the 2 boards. I would then like to terminate the connection. ...
Hello,I have found some bugs in linker scripts generation when creating a project from CubeMX. Those bugs appears only when code is generated for STM32CubeIDE, related to linker scripts:/* Highest address of the user mode stack */ _estack = 0x2004000...
In STM32CubeProgrammer I can set RDP on AA level and BB level, but in CLI mode read/write protection is constantly in BB. In CLI protection byte doesnt change, I mean I can't change itand can't write FUS or stack, and even check the fuse version.C:\P...
I have successfully uploaded stm32wb5x_FUS_fw.bin to my STM32WB55CC and the next step resulted in the error I don't know how to deal with. Here is the CMD log ------------------------------------------------------------------ ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.