STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

STM32F411 and P-NUCLEO-LRWAN1 (SX1272MB2DAS)

Hi,I'm trying to run ping pong example in f411 board with sx12mb2das module but it doens't work and I don't know why (I have b-l072z-lrwan running as receptor). Has anybody ran the program in that board?Thank you.

Larraitz by Associate II
  • 2218 Views
  • 4 replies
  • 0 kudos

Recieve only txdone, onrxtimeout,ontxdone

Hi. I have a brand new STM32 LORA and SIgfox discovery kit. I try to send any AT-command but i Only/always recieve txdone, onrxtimeout,ontxdone what is wrong???Best regardsBjarne

BToft by Associate II
  • 830 Views
  • 0 replies
  • 0 kudos

Problems in debug I-CUBE_LRWAN in PINGPONG MODE.

Hello everyone, I am debugging my stm32L073+sx1272 in the pingpong mode. I run the program in debug mode. I know that there is a while loop and the "state" variable should be the variable to implement different functions such as TX RX RX_TIMEOUT and ...

mlau.18 by Associate II
  • 1023 Views
  • 1 replies
  • 0 kudos

Resolved! Border Router with Thread Network

Are there any application notes or references about a border router used with a Thread network because I hadn't found any.

NGama by Associate III
  • 1822 Views
  • 3 replies
  • 0 kudos

Resolved! Pulse Density Modulation Interface

Hi!I'm trying to enable the PDM interface on a STM32WB55RGV with one microphone. Basically i followed the AN5027 application note, but I'm not able to start the clock on the proper GPIO. The configuration from CUBE-MX seems ok, and I checked the reg...

0690X00000AqXgJQAV.png 0690X00000AqXgOQAV.png

STM32WB55RG : Flash memory available for user application

Hi all,I'm trying to determine how much FLASH memory will be available for my user application. I'm using an STM32WB55RG. I don't do this quite often so I could use some helpI got clues from different sources but i'm not sure which one is correct :Gi...

Steven.D by Associate II
  • 5649 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.