STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Exchange strings between Server and Node

Hi everyone,I have built two custom ​boards (One server and and one node) and my application requires that the server and client communicate with each other and exchange the following parameters.A name in stringDate day and time.​The server will send...

AKetc by Associate III
  • 2016 Views
  • 6 replies
  • 0 kudos

How to make ble characteristic payload more than 20 chars?

Hello,I want to make payload with 32 chars in my ble servise, I'm changing it in p2pstm.c like in workshop, but nothing more than 20 chars does't transmits. Also allready tried to change the ATT_MTU value in appConf.h - didn't help. How to do it?

PHerm by Associate
  • 1324 Views
  • 1 replies
  • 0 kudos

I-CUBE-LRWAN Software Expansion 1.3.0 Does not work

I have loaded SE 1.3.0 out of the box (only changed app and dev ids) onto a Nucleo board, and after a few uplinks (data) the loraserver does not send a downlink confirmation, as if the fcnt is incorrect. In fact the fCnt is OK. It could be that the M...

GChis by Associate
  • 685 Views
  • 0 replies
  • 0 kudos

Writing a program to the controller

Hi). I made a minimal design for STM32WB55 on board. This board has 3 program pads. There ara GND, SWDIO, SWCLK. Сontroller current is 11mA at the factory program. I try to flash the controller using these contacts, but nothing works. I use ST_LINK (...

Sasha2 by Associate II
  • 3095 Views
  • 9 replies
  • 0 kudos

Set Up Communication Between ESP8266-01 and NUCLEO-F030R8

I've been tasked with figuring out how to get a mobile app to communicate with an MCU then in turn control a stepper motor. Right now I'm trying to get the WiFi module (ESP8266-01) and MCU (NUCLEO-F030R8) to play nice with each other. The catch is I ...

SNeub by Associate II
  • 1257 Views
  • 0 replies
  • 0 kudos

Resolved! Failed to read memory after RDP set/reset

I'm trying to program BLE stack on a custom board based on STM32WB55CG. I'm using SWD, CubeProgrammer 2.2, CubeFW_WB 1.1.1.First I've successfully performed -fwdelete. But then I got "Firmware not authentic" error trying to make -fwupgrade. So I've s...

Stecklo by Senior
  • 3180 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.