NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
We have developed an IoT sensor using the STM32WLE5JC LoRa module. It is a device we expect to reboot a few times (when necessary). It was discovered that when a downlink command (to reboot the device) is sent, the device reboot, but then it hangs d...
Hello everyone,I’m working with an STM32WLE5CCU6 and I have implemented a bootloader that should be able to start applications stored in two flash regions (“slots”).Bootloader at 0x08000000Slot 1 (FW1) at 0x08005000Slot 2 (FW2) at 0x08015000Applicati...
I'm developing a Sigfox product using the STM32wlxx series.For testing purposes, I'm trying to provision Sigfox using the STM32 programmer,but I can't log in using the link https://my.st.com/cas/login?service=https://my.st.com/sfxp.
Hello,I wrote a custom bootloader (that loads firmware image from an external flash) for a device that was using an STM32WL55CCU6. Now I want to use the same bootloader on a device with a similar uC, the STM32WL5MOCH6TR.The bootloader works correctly...
I'm currently tinkering with the BLE_Ota example for the P-NUCLEO-WB55.Nucleo and created a debug build spec for it. The default linker script is /* Specify the memory areas */ MEMORY { FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 28K ...
Hi everyone, I'm experiencing abnormal power consumption in STOP2 mode with my custom board featuring the STM32WB5MMGH module. According to the datasheet, the power consumption in STOP2 mode should be between 2 and 3 µA. However, my board is drawing ...
Hello Together,I would like to try out the STM32CubeMonitor-RF (V2.15.0) with the NUCLEO-WBA55CG board. I downloaded the stm32cubewba mcu package (V1.7.0) and flashed the .bin file from the BLE_TransparentMode example to the board with the STMCubePro...
We need some help with cable replacement feature. Our project using WB1M as a client device, sharing data over UART. Android application must be server. STBLESensor_Android source code not include any sample code with Cable replacement feature. Were ...
Hello, @STTwo-32 I am working with the NUCLEO-WB05KZ (MB1801 + MB2032B target). I received two boards from the ST eStore. One board works fine: STM32CubeProgrammer detects the target, and I can erase/flash/debug with no issue. The second board ini...
Hello everyone,I am working with a custom board based on the STM32WB5MMG. On the very first attempt, the FUS firmware update works fine and completes successfully. The problem starts when I try to update the FUS again. Once it has been updated for th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.