NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Split from Interfacing external sensors with I-CUBE-LRWAN End Node STM32L476RG based Library.Hi! Could you please share how you interfaced the RFM95 with the STM32L476RG using the I-CUBE-LRWAN library? I’m new to using the I-CUBE-LRWAN library and wo...
Using STM32CubeWB v1.23.0, I am running the hardware timer in the following order:HW_TS_InitHW_TS_CreateHW_TS_StartHowever, despite this, the callback registered at the time of Create is not executed after the set time.What could be the problem?
Hello,I have a question regarding the antenna area PCB artwork design for the STM32WB1MMC and STM32WB5MMG modules.In the STM32WB5MMG datasheet, it is recommended to:- place the module at the edge of the PCB,- fill the right-hand side of the module wi...
We are seeing an issue where the STM32WB55 module is failing to send a valid write response. The write response is attempted but based on the packet logs, the CRC is failing. This results in the central (app running on Android) forcing a disconnect...
Hello STM Community, I’ve successfully implemented a Zigbee application on the STM32WB series MCU that leverages the Low Power Manager to enter Standby or Shutdown modes, as detailed in AN5289 section 4.6. The application note highlights the Low Powe...
Hi, I'm planning to use a STM32WB5MMG for a custom board. For this application, I need to measure the frequencies and the duty cycles of three different PWM signals. I know that there is the PWM Input mode of some TIM. However, I verify that there ar...
Hello everyone,I'm currently working with the STM32WBA65RI Nucleo board.For my upcoming application, I require a stable BLE throughput of over 800 kbps. However, using the provided example, I can only achieve around 600 kbps.So far:I'm using an MTU o...
Hi.I'm working on stm32wb for some time, handling CPU2 updates of BLE stack application.Lately, version 1.23 was published with new FUS version, so I tried updating it with my application running on user flash. I searched for the magic word but I fou...
Hello everyone,I’m working with an STM32WB55 microcontroller with BLE stack. I use also low-power modes in my app. Before entering a low-power mode, I set an RTC ALARM_A to wake the system up at a specific time. The device then enters either Sleep or...
Hi,I want to integrate on the same PCB both a STM32WB5MMGH6TR and a STM32WL5MOC. Are there any issue in terms of RF interference? Are there any shielding recommendations to avoid problems while both modules are transmitting?ThanksMatteo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.