NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
When using the Custom Template option in Cube MX 5.6 for the WB55, the generated "custom_stm.c" file contains some bugs in the "Custom_STM_App_Update_Char" function. Namely, the calls to "aci_gatt_update_char_value" mistakenly pass the characteristic...
HiI am trying to generate a true random number on the B-LO72Z-LRWAN1 using the HAL_RNG_GenerateRandomNumber function with the code below:uint32_t rnd_generator (void) {RNG_HandleTypeDef RngHandle; // RNG handler declaration uint32_t rv; RngHandle.I...
Hi,Can any one guide me how can i enable debug messages in BLE_HeartRateFreeRTOS demo.i have enable below macro but doesn't get any success#define CFG_DEBUGGER_SUPPORTED 1#define CFG_DEBUG_BLE_TRACE 1#define CFG_DEBUG_APP_TRACE 1#define CFG_DEBU...
Hello,I successfully able to download and run the BLE_OTA example (on WB55-Nucleo platform)I had transfer the M4 FW file only, named: BLE_p2pServer_ota_reference.bin with the size of 33.6KB, The Total transfer time was: 42.02 Sec (on my Huawei p10 m...
Greetings, I have my STM32WB55RGV6 connected to my computer through USB using the ST-LINK port on the board. When trying to flash the coprocessor to run an example application from the WB firmware package, I cannot even erase the previous firmware. U...
Using STM32CubeMonitor-RF I am able to update my device via OTA with one small issue. I send the command to program my device and my application gets deleted and the device reboots into our OTA application but I have to search for my device a second ...
Hiat_master software works fine but end_node software not working I tried OTAA and ABP.
I have a project using the STM32_WB55 where I use CubeMX to setup a custom BLE template, services, characteristics, etc. I noticed that STM32Cube_FW_WB_V1.8.0 supports both BLE and FREERTOS, but when I enable FREERTOS, all my custom BLE settings are ...
STM32WB SoCs have radio module. I need a way to write own wireless stack but the documentation is lacking their description.So far documentation mentions 3 peripheral devices on APB3:0x6000 1000 - 0x6000 1FFF 4 KB 802.15.4 CTRL0x6000 0400 - 0x6000 07...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.