STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB sequencer bug?

Hi,I'm using CubeMX to generate the code for the STM32WB and I found a problem in the secuencer library which is automatically generated.When I register a new task in the scheduler, this places the callback function in TaskCb[0] but when I set the ta...

Diego B. by Associate II
  • 2848 Views
  • 4 replies
  • 0 kudos

B-L072Z-LRWAN1 with sleep-on-exit feature

Hi there, I'm using a customized board based on B-L072Z-LRWAN1. I also use I-CUBE-LRWAN (v1.1.4), compiled on Keil uVision. Everything works fine. I can get about 2uA in Stop mode. Now I'm doing a project requiring power consumption optimized so I en...

JLe.1 by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMx generating sources with errors

I am trying to initiate a project via cubeMx for the STM32WB55 nucleo board.I an able to initiate a simple project without the BLE middleware (STM32_WPAN).Once adding the STM32_WPAN, the generated project not compiled on both Atollic true studio and ...

~Amit~ by Associate III
  • 4534 Views
  • 9 replies
  • 0 kudos

Error upgrading wireless coprocessor firmware on Nucleo-68

I am experiencing an error while trying to upgrade a Nucleo-68 board from P-NUCLEO-WB55 wireless coprocessor to latest v1.7.0 firmware provided by STMicroelectronics/STM32CubeWB github repo.I already reported the issue on the githb repo here is a cop...

anddam by Associate II
  • 4560 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.