NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Is it possible to start USB host on STM32WB55 MCU?
Is there any public examples of a stm32wb Bluetooth client application. Where the stm32wb client does a few read's and write to a server bluetooth applicaion. What i was thinking of was a BLE_HeartRate_Client program to the BLE_HeartRate program ...
In Group 1 G1_IO4 is a sampling capacitor and G1_IO3 is a sheild and in Group 2 G2_IO2 is sampling capacitor and G2_IO1 is input touch key. In Group 3 G3_IO4 is a sampling capacitor and G3_IO2 is a input touch key. so when i programmed with this conf...
Hello! I'm working with an STM32WB55 development board and I'm trying to take data fairly quickly (every 25 us) so I'm trying to work with the DMA to collect data. Right now, I'm not even collecting actual ADC data, just toggling a GPIO point to ge...
When receiving a write event to a characteristic via Bluetooth it is possible to return SVCCTL_EvtAckFlowDisable from the service handler.This then results in the event buffer not being released back to CPU2.But what happens if CPU2 runs out of memor...
Hello, I'm working on STM32WB55.Is there any limitation to write to (internal) SD RAM and do a system reset?I want to build an application that requires a lot of writing to SD RAM and then do system reset (and read the SD RAM and act according the da...
I have a B-L475EIOT01A2C evaluation board. Is it possible to use the LoRa software expansion for STM32Cube in order to address the SX1272 MBed Shield (SX1272MB2xAS) which fits on the evaluation board?
arm-none-eabi-gcc -o "P2P_Server.elf" @"objects.list" -lbep_diag_hf -lbep -lbep_diag -lbep_hf -mcpu=cortex-m4 -T"D:\kiran\new1\p2p\P2P_Server\P2P_Server\STM32CubeIDE\STM32WB55RGVX_FLASH.ld" --specs=nosys.specs -Wl,-Map="P2P_Server.map" -Wl,--gc-secti...
Hello, please be warned, I am ultra new to STM32 mikrocontrollers (student).I watched several hours of tutorials and now I am starting my first steps in programming. I am using the CubeMX to set up the code.Unfortunately, I can´t get the USART1 runni...
Hello,I am currently testing the P-NUCLEO-LRWAN2. I am having problems getting it to work. I followed the tutorial in the UM2073. I managed to perform all the steps requested but I don't receive any data in the LORIOT dashboard.I also uploaded the "E...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.