2020-08-23 10:57 PM
Hello,
I successfully able to download and run the BLE_OTA example (on WB55-Nucleo platform)
I had transfer the M4 FW file only, named: BLE_p2pServer_ota_reference.bin with the size of 33.6KB, The Total transfer time was: 42.02 Sec (on my Huawei p10 mobile running "ST BLE Sensor" mobile App. v4.7.1)
Meaning the Transfer Rate is less then 10Kbits/Sec
Please advise why the Transfer Rate is so slow? and what need to do in order to make it faster?
Thanks In Advance,
Micha
2020-08-24 2:45 AM
Most of the mobiles have a fixed and limiting connection interval as Bluetooth parameters. so it is difficult to show the real OTA performances with a mobile.
I did the same experiment with my mobile (Samsung A5) and I get the download doe in 32.17s which is still a quite low bit rate compare to the expected max throughput.
You could try the CubeMonitor-RF tool that get a higher bitrate as the connection interval can be easily modified.
2020-08-24 2:50 AM
Remi,
Thanks A Lot for your prompt reply
Micha
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.