STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! HAL_UART_Receive_DMA randomly stops working?

I am working with an STM32WB5MMG, but I don't think this issue relates to the radio part of the MCU, so I am posting in the more general community. I hope that's okay.I am reading data from a GPS receiver over UART using the HAL_UART_Receive_DMA func...

crwper by Senior
  • 3922 Views
  • 4 replies
  • 0 kudos

CMWX1ZZABZ with STM32CubeExpansion_SFOX_V1.1.0 blocks on TX_START unless PA2 and PA3 are physically pulled up and configured as LPUART

Hi,I have tested a B-L072Z-LRWAN1 board with the default Sgfx_push_button application included in STM32CubeExpansion_SFOX_V1.1.0 folder. So far so good, everything was working as expected.I've designed and built a custom board, following the requirem...

NUCLEO-55WLJC1: Most Elemental HAL Functions Don't work

Hey guys, I'm Working on the NUCLEO-55WLJC1 Board. My Problem seems very simple but I've been struggling with this for some time now. I want to use HAL_GPIO_TogglePin To toggle a pin, but it has no effect at all. I tried to use HAL_GPIO_WritePin inst...

0693W000007EKhuQAG.jpg
MSchn.3 by Associate II
  • 1126 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.