NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I have a STM32WB55-Nucleo running the BLE_HeartRateFreeRTOS sample application. All works well for a while - I can scan and connect to it (from LightBlue on iOS) and read, write and subscribe to notifications. However, after approximately 40 mins,...
Hi everyone,I am developping an application on the SPBTLE-1S module (BLE 4.2).When the connection quality is low, a disconnection will sometimes occur with error code 0x28 (Reason: Instant Passed) before the connection timeout is reached.Current conn...
I am trying to build a Lora-End-Node application for STM32L476RGT6 + a separate Semtech SX1272 chipt attached to it. The only exampüles are for Nucleo boards. In addition the code is stringly nested, so that it is difficult to understand. ST sure did...
Hi,I am trying to develop a ble application with the stm32wb55 and stm32cubemx. The MCU is on st nucleo board.I have create a new cubemx project, add middleware BLE STM32_WPAN, add scheduler on while() cycle in main.c, add IPCC interrupt handlers in ...
A new version 2.7.0 is released.New features :802.15.4 RF sniffer : it is now possible to use a STM32WB Nucleo boards to spy the 802.15.4 packets and display the traces in Wireshark. Wireshark can be started directly from STM32CubeMonitor-RF. The pr...
Dear ST-Community,I've checked your latest Ressources on STM32WLE:https://www.st.com/en/microcontrollers-microprocessors/stm32wlex.html#cad-resourcesAnd opened the file in Altium to export it to P-CAD ASCIIhttps://forums.autodesk.com/t5/eagle-forum/i...
Hi, I tried the LocalNetwork demonstration in which one NUCLEO board acts as a concentrator and other NUCLEO boards act as sensor unit. Its available in STM32Cube_FW_WL_V1.0.0/Projects/NUCLEO-WL55JC/Demonstrations/LocalNetworkI loaded and ran one NUC...
Can someone tell where I can find an ioc file for BLE_MeshLightingPRFNode application ? I am using STM32WB55RG and SDK version is 1.8.0. I see that ioc file is available for every example and BLE application but not for the above application. What is...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.