STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB50 RTC counts more than 24h

Hello, I'm using STM32WB55 for my application.My application is installed in 20 devices more or less.I set the RTC with RTC_HOURFORMAT_24.The RTC calendar is updated every 24 hours by cloud, usually.Only two of those devices, expose a problem with RT...

Having trouble using B-L072Z-LRWAN1 to communicate to The Things Industries through gateway because of 5 minute timeout/nothing received.

I have a B-L072Z-LRWAN1 development board and am using it to send a PWM (0-100%) value to TTI and receive a PWM value to control a fan. The LoRa settings at the moment are:Class C deviceADR off (using DR_3)Confirmed uplinksNo periodic uplinksThe prob...

CMets.1 by Associate
  • 839 Views
  • 0 replies
  • 0 kudos

Teams problems

Please forgive me for not attending the workshop, but I couldn't force Teams to cooperate.I had to go through at least 10 email and passwords resets and best i got to wasAADSTS50020: User account '--@---------.---' from identity provider 'live.com' d...

TJaku.2 by Associate II
  • 1521 Views
  • 2 replies
  • 0 kudos

Can't get the advertising state

Hello everyone,I'm trying to build a server application with the STM32WB55 but I can't get the advertising state. I took example on the server example in the STM32Cube_FW_WB_V1.0.0 and I think it is pretty similar but it doen't work as intended. I ma...

Franklin by Associate II
  • 7966 Views
  • 13 replies
  • 0 kudos

Sychronize time with LoRa Network using STM32WL

Hi all,How can I launch a request to synchronize the date/time at the application level using the LoRa's Stack that the STM32WL uses?I have seen that there is a function to launch that request, but it is not accessible at the application level since...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.