2021-03-10 10:28 PM
Hi all,
How can I launch a request to synchronize the date/time at the application level using the LoRa's Stack that the STM32WL uses?
I have seen that there is a function to launch that request, but it is not accessible at the application level since it is defined in the .c but not in the .h
LmHandler.c <<LmHandlerDeviceTimeReq()>>
Is there any way to call this function without modifying the code
Best Regards,
Sergio
2021-03-17 10:39 PM
Hi all,
In order to set the time synchronizing with the network, what I have had to do is:
Put the function LmHandlerErrorStatus_t LmHandlerDeviceTimeReq(void); in the .h to give it visibility
And when I want call this fuction before LmHandlerSend() to make the synchronization
I don't know if it's the correct way
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.