NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
The documentation for STM32WB55 Nucleo states that a 5.2 stack is available ("comes with") but the BT stack provided in STM32Cube_FW_WB_V1.11.0 is a 5.0 stack...Regards,AC
Hi,I received my kit and saw that the package was damaged in some place. After powering on NUCLEO-L073RZ, no obvious problem (LED are OK).On NUCLEO-F746ZG, everything seems OK too (LED OK)On LRWAN_GS_HF1, no LED turns ON. If I understand well, at lea...
Hello,We are finalizing the low power modes of our project and can't manage to solve this issue.We are going correctly into Low Power Mode via the UTIL_SEQ_Idle and related functions...But it looks the CPU2 (BLE) doesn't wake up the CPU1.Our applicat...
Hello,I'm struggling with BLE scanning on an STM32WB55 based application as GAP_CENTRAL_ROLE.We need to scan for beacons, and can't see any with ADV_NONCONN_IND, if device Advertises as connectable everything works perfectly.Any suggestions welcomed....
since the board has Lora embed with the kit. i want was set up the rf connectivity to transfer data between two such device.Any one please guide me with setup and code
I want to enable Terminal I/O using SWO for printf() function. I can't figure out why Iit doesn't work on that examples. It work on other examples (FreeRTOS and HAL Template).I follow the instructions from the IAR EW app manual and it doesn't worked....
The button "Join the workshop" in the email is just a download link for a calendar invite, not an invitation to a teams meeting or similar.
Hi STI'm right now preparing for the WS tomorrow and would like to setup my system so I'm ready. One issue I face is this part:This is under "Network connections configuration" Proxy entries for HTTPHTTPS and SOSKS.Thank you in advance :)BRLars Munch
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.