STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32 UART HAL and LL failed

Sorry ST guys but the UART HAL and LL_HAL ist a total fail!I developing over 15 years all kind of serial communication with linux and different microcontrollers. Now I regret my desistion to use the STM32WB MCU. I'm trying over two weeks the get a st...

STUser21 by Associate II
  • 4584 Views
  • 9 replies
  • 0 kudos

ST bluenrg2 low power current consumption

I am developing a Beacon model application with ST bluetile. Bluenrg2 low power current consumption differs between SensorDemo (200uA) and Beacon application (1.8mA). I made sure that the bluetile goes into SLEEP_NO_TIMER mode and wakes up only when ...

SMano by Associate II
  • 748 Views
  • 0 replies
  • 0 kudos

Problem using the internal Flash using P-NUCLEO-WB55

Hi,I'm using the example FLASH_WriteProtection with P-NUCLEO-WB55 with success but if I change the define FLASH_USER_START_ADDR in order to write only two (so I change the define FLASH_USER_END_ADDR  in   'ADDR_FLASH_PAGE_250 + FLASH_PAGE_SIZE - 1') ...

GPomp.1 by Associate III
  • 2641 Views
  • 6 replies
  • 0 kudos

Slow speed with BLE throughput example

With the throughput example if i use 2 WB55 boards, the maximum throughput that i get is 2KBpsDT = 2160 bytes/s lost = 0If i use my phone with PHY1, i get 90KBps+ and with PHY2 sometimes its 150KBps and sometimes 15KBps, on download. With upload its ...

G5658 by Associate III
  • 860 Views
  • 0 replies
  • 0 kudos

Not getting interrupt from CPU2 to begin advertising state.

It seems I am having the same problem here: https://community.st.com/s/question/0D50X0000Az4HdhSQE/cant-get-the-advertising-state?t=1613668936202. Except the solution for that question was to make sure the memory buffer was mapped properly to SRAM2 a...

Louis1 by Associate II
  • 2953 Views
  • 5 replies
  • 0 kudos

STM32WB55 unable to modify option bytes.

1. STM32WB55 unable to modify option bytes.2. It is not even allowing to do full chip erase. 3. M4 is running but M0 is not running hence it is struck at IPCC Initilization.

YSN by Senior
  • 702 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.