NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
智能穿戴产�?带�?牙5.0的芯片有没有推�??的?�?牙芯片 [�?制链接]这个�?牙芯片我们希望集�?更多的功能,比如内存有1M以上;有ADC采样,有OP�?放,或者内置有AFE电路;有充电管�?�(如果没有�?�以增加充电芯片,本身充电芯片体积�?会很大);需�?5.0或以上版本;带电�?监测功能或者�?�以外挂电�?计芯片;有串�?�或者IIC接�?�;这样的过功能�?牙芯片有没有�?�适的或者接近的?类似一个SOC的功能
Is there a way to send a single advertisement packet at a specific moment in code, ( without the mix/max interval time).I want to disable advertisement.And control it myself.
Hi, For my application, I have BLE connection between STM32WB55 (role = peripheral ) and mobile connection.I want to use BLE in low power mode such a way that, 1) If device is not paired MCU(M4) should wakeup and pair if device is available then slee...
Hi, I'm using a custom board with STM32WB55 and faced with an issue related to FUS up and running. Initially, I was able successfully to upgrade FUS up to 1.1.2.0 via swd interface. Then I have updated the user key via USART embedded bootloader. Star...
I am working on the Programmable Voltage Detector (PVD) and was wondering if I can decrease the voltage instead of the default 3 volts it is outputting right now. I would like to decrease in different intervals to test the PVD.
HELLOI have a custom board with STM32WLE5J8I MCU and i want to make a LORAWAN End Node applicationI don't find any tutorial or video explaining step by step how to do this Thank you
Hi,I'm trying to swap the TX/RX pins of UART but I can't make it happen without the project configuration file that is not present in the Zigbee_SE_Msg_Server_Router project.I tried to change the pins in the 'hw_conf.h' file but that doesn't seem to ...
This is the data I grabbed with bushound. As shown in the picture, when I send data through HID once, the USB will send empty data packets indefinitely, and subsequent data packets will cause the transmission to be stuck and repeated. I tested the US...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.