2021-06-08 8:25 PM
智能穿戴产�?带�?牙5.0的芯片有没有推�??的?
�?牙芯片 [�?制链接]
这个�?牙芯片我们希望集�?更多的功能,比如内存有1M以上;有ADC采样,有OP�?放,或者内置有AFE电路;有充电管�?�(如果没有�?�以增加充电芯片,本身充电芯片体积�?会很大);需�?5.0或以上版本;带电�?监测功能或者�?�以外挂电�?计芯片;有串�?�或者IIC接�?�;这样的过功能�?牙芯片有没有�?�适的或者接近的?类似一个SOC的功能
2021-06-08 10:57 PM
Google translation as:
Is there any recommendation for smart wearable products with Bluetooth 5.0 chips?
Bluetooth chip [Copy link]
We hope to integrate more functions of this Bluetooth chip, such as memory with more than 1M; ADC sampling, OP amplifier, or built-in AFE circuit; charging management (if there is no charging chip can be added, the size of the charging chip will not be very large Large); version 5.0 or above is required; with current monitoring function or an external fuel gauge chip; with serial port or IIC interface; is there such an over-function Bluetooth chip that is suitable or close? Similar to a SOC function
2021-06-09 2:30 AM
看�?懂 都是英文�?�
2021-06-09 3:02 AM
Hi,
General language of this community is English. If you want to successfully participate (receive answers) I recommend to use English. Maybe you can use translation service like Google translate.
-- Google Translate -->
这个社区的通用语言是英语。 如果你想�?功�?�与(收到答案)我建议使用英语。 也许你�?�以使用�?谷歌翻译这样的翻译�?务。
此致
Best Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.