NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am trying to send a BLE notification after I have connected. I add the characteristic this way. retVal = aci_gatt_add_char(serviceHandle, UUID_TYPE_128, (const Char_UUID_t *)Uuid, ...
I have a board with an STM32WLE5CC and am attempting to use STOP2 mode, but instead of the expected 4-6uA I am seeing 1mA consumption.All peripherals except FLASH, HSEM, and the RTC are disabled in the RCC block. All Unused GPIO are set to Analogue. ...
HiI don't understand how to use the custom bluetooth template in CubeIDE for a STM32WB55CC microchip. I need to know how to configure this in order to understand how to configure a bluetooth liaison with BLE.Best regards
I have followed instructions from many threads but none seems to work. I am not sure if I tweaked the Anti-Rollback before a FUS update. Please help.So is there a way to revive my board ??If I have bricked my board and cannot REVERT back I need to k...
Development Environment: KEIL (Free License)보드 : DISCO-L072CZ-LRWAN1HelloTo build a monitoring system with the LoRa protocol now.It is being developed as a 'DISCO-L072CZ-LRWAN1' board.I turned off the 'ST-LINK' built into the board to check the min...
Could you get the binary data of STM32 of LRWAN3 which is loaded in NUCLEO-LRWAN3 by default?thank you for your help..*Moderation Edit: please do not post your email in the public area of this website*
Can anyone tell me what Update_Type parameter does in this fucntion?tBleStatus aci_gatt_update_char_value_ext( uint16_t Conn_Handle_To_Notify, uint16_t Service_Handle, uint16_t Char_Handle, ...
HiUsing a P-NUCLEO-WB55 dev board.Looking for a dedicated ST Windows app to debug BLE .Something that maybe connects to the ST USB dongle, and can run simple commands as connect, pair etc.Is there such a tool available?similar to this, but for window...
Using STM32WB, testing pairing-bonding. Using several BLE dongles for desktop PC.Peripheral - ST. (APP HeartRateRTOS example )Client - Windows 10 , BLE debug dongles.After pairing and bonding I read the bonded devices using:aci_gap_get_bonded_devices...
NUCLEO-LRWAN2�?� sensor 보드�?� 기본 �?재�?� firmware�?� souce code가 있으면 보내 주시면 �?사하겠습니다. i want a firmaware of F746RZ.STM32CubeExpansion_LRWAN_V2.0.0는 가지고 있는�?� 혹시 �?�것�?� 맞으면 어떻게 compile 해야하는지 알여주세요My project is breaking up.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.